An ADS and ADX on the same site - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 13.0

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document number
LIT-1201645
Version
13.0
Revision date
2023-10-12
Product status
Active

While it is possible to install both an ADS and an ADX on the same site (with the restriction that an ADS-Lite cannot be the Site Director for any other ADSs or ADXs), historical data cannot be shared between the two computers. The repository files only exist on one ADS/ADX computer or on the database server computer in the split ADX. The Engines can send historical records to only one repository computer.