Site time server - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 13.0

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document type
Commissioning Guide
Document number
LIT-1201645
Version
13.0
Revision date
2023-10-12
Product status
Active

As an alternative to setting date and time manually for a device, you can select a site time server. A site time server sets the date and time in the Site Director. If you have a split ADX, select the same site time server for both the web/application server computer and the database server computer. Site time servers can be on your intranet, such as a Domain Controller/Server; or on the Internet, such as the U.S. Naval Observatory Master Clock.

For a list of Navy master clocks, go to https://www.usno.navy.mil.

See Selecting a site time server for the Site Director ADS/ADX (Windows method only) sections.