Appendix: Installing antivirus software - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 13.0

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document number
LIT-1201645
Version
13.0
Revision date
2023-10-12
Product status
Active

To install antivirus software on computers that run Metasys software, complete the steps in this appendix. Use one of the following antivirus software programs:

  • Symantec® Endpoint Protection software Corporate Edition version 12.x or later.
  • McAfee® VirusScan® Enterprise version 8.8 with Patch 9 or later.
  • Windows® Defender Antivirus® built into Windows® 11, Windows® 10, Windows® Server® 2022, and Windows® Server® 2019.