Removing user preference files - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 13.0

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document number
LIT-1201645
Version
13.0
Revision date
2023-10-12
Product status
Active

Procedure

  1. Access the Metasys device from which you want to remove the user preference files and navigate to the Preferences directory for the device as shown in Table 1.
  2. Delete files named UserPreferences-userID.xml, where userID is the identification number that appears in the Security Administration tool.
    Note: Do not delete DefaultUserPreferences.xml.