Restarting the Metasys Server services and application pools - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 13.0.50

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document type
Commissioning Guide
Document number
LIT-1201645
Version
13.0.50
Revision date
2024-02-26
Product status
Active

About this task

To run the restart batch file from the system utilities, follow these steps:

Procedure

  1. Browse to C:\ProgramData\Johnson Controls\MetasysIII\Diagnostics\Utilities.
  2. Right-click on the restart.bat and select Run as Administrator. Click Yes in the User Account Control dialog box. A Command Prompt windows appears and displays the status of restarting the services. When the services start, the Command Prompt window closes.