The following information is new or revised:
- Updated support for SQL Server® 2022 with CU9 (64-bit)
- Updated support for SQL Server® 2022 Express with CU9 (64-bit)
- For more information on these updates, see Technical specifications.
-
Note: Make sure that you enable and configure proper certificate revocation, such as Online Certificate Status Protocol (OCSP) stapling. For more information about OCSP configuration refer to https://docs.microsoft.com/en-us/openspecs/windows_protocols/ms-ocsp/5792b4c4-c6ba-439a-9c2a-52867d12fb66.