Creating audit entries for discard events - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 13.0.50

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document number
LIT-1201645
Version
13.0.50
Revision date
2024-02-26
Product status
Active

About this task

By default, the ADS/ADX does not create an audit entry when you discard an event that originates on the ADS/ADX.

Note: Network Engines do not create an audit entry when you discard events that originate on the engine. For details on changing this setting, refer to the NAE Commissioning Guide (LIT-1201519).

Procedure

  1. On the ADS/ADX computer, right click Notepad and select Run as administrator.
  2. Using Notepad, open the following file:

    C:\Program Files (x86)\Johnson Controls\MetasysIII\WS\web.config

  3. Find the line for WriteAuditAckDiscard:

    add key="EventRepository.WriteAuditAckDiscard" value="false"/

  4. Change the value from false to true.
  5. Save the file and close all windows.
  6. Restart the ADS/ADX.