Use one of the following configuration options:
-
The ADS/ADX is the Site Director and the ADS repository.
-
The ADX is split configuration that supports the web or application server computer is the site director, and the database server computer is the repository.
- Open the ADS object or device you plan to modify.
- Set the object or device according to Table 1.
|
Condition |
Device or Object |
In This Field |
Enter This Value |
|---|---|---|---|
|
If the ADS/ADX is Both the Site Director and the ADS Repository |
On the ADS/ADX (Site director) |
ADS Repositories |
Not used. leave blank |
| On a network engine |
Local Site Director |
The computer name/IP Address of the Site director ADS/ADX | |
|
ADS Repository |
|||
| On any other ADS |
ADS Repositories |
||
|
If the ADX is Split and the Web/Application Server Computer is the Site Director and the Database Server Computer is the Repository |
On the ADS/ADX (Site director) |
ADS Repositories |
Not used. leave blank |
| On a network engine |
Local Site Director |
The computer name/IP Address of the Web/Application server computer | |
|
ADS Repository |
|||
| On any other ADS |
ADS Repositories |