Spaces authorization repository database overview - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 13.0.50

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document number
LIT-1201645
Version
13.0.50
Revision date
2024-02-26
Product status
Active

The Spaces Authorization Repository resides on the ADS/ADX, within the SQL Server software database. The folder location of the database files that store spaces authorization data is selected during the Metasys server installation. The default directory location is C:\Program Files\Microsoft SQL Server\MSSQL<version>.MSSQLSERVER\MSSQL\DATA (Release 8.0 or later). The Spaces Authorization database stores the Metasys UI Advanced Search & Reporting Reports.

Note: The installation program places the Spaces Authorization repository on the same computer where the ADS/ADX software resides. For a split ADX, the directory location is on the database server on the same drive where the SQL Server software is installed. If you want to change where the databases are loaded (for example, E:\MyDatabases), you need to do so before you install the ADS/ADX software. For details, refer to the Custom Locations for Metasys Server Application and Databases section in the Metasys Server Installation and Upgrade Instructions (LIT-12012162).