Metasys UI reporting repository database overview - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 13.0.50

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document number
LIT-1201645
Version
13.0.50
Revision date
2024-02-26
Product status
Active

The JCIReporting database for Metasys UI is used for the custom trend viewer and resides on the ADS/ADX/OAS/NAE85/LCS85 within the SQL Server Software database. The folder location of the database files that store trend data is selected during the Metasys server installation. The default directory location is C:\Program Files\Microsoft SQL Server\MSSQL<version>.MSSQLSERVER\MSSQL\DATA (Release 8.0 or later).

Note: The installation program places the Metasys UI Reporting repository on the same computer where the ADX software resides. For a split ADX, the directory location is on the database server on the same drive where the SQL Server software is installed. If you want to change where the databases are loaded (for example, E:\MyDatabases), you need to do so before you install the ADS/ADX/OAS/NAE85/LCS85 software. For details, refer to the Custom Locations for Metasys Server Application and Databases section in the Metasys Server Installation and Upgrade Instructions (LIT-12012162) .