The JCIReporting database for Metasys UI is used for the custom trend viewer and resides on the ADS/ADX/OAS/NAE85/LCS85 within the SQL Server Software database. The folder location of the database files that store trend data is selected during the Metasys server installation. The default directory location is C:\Program Files\Microsoft SQL Server\MSSQL<version>.MSSQLSERVER\MSSQL\DATA (Release 8.0 or later).
Note: The installation
program places the Metasys UI Reporting repository on the same computer where the ADX
software resides. For a split ADX, the directory location is on the database server on
the same drive where the SQL Server software is installed. If you want to change where
the databases are loaded (for example, E:\MyDatabases), you need to do so before you
install the ADS/ADX/OAS/NAE85/LCS85 software. For details,
refer to the Custom Locations for Metasys Server Application and
Databases section in the
Metasys Server
Installation and Upgrade Instructions
(LIT-12012162)
.