Event repository optimization - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 13.0.50

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document type
Commissioning Guide
Document number
LIT-1201645
Version
13.0.50
Revision date
2024-02-26
Product status
Active

Optimize the required storage size of the ADS/ADX Event repository by only defining intrinsic alarming, Event Enrollment objects, or alarm extensions for point objects for which event messages need to be processed and archived.

In addition, optimize the network communication performance for transferring event messages from engines to the ADS/ADX Event repository by optimizing the Alarm repository size in the device object of each engine.

Refer to the Alarm and Event Management section in the Metasys SMP Help (LIT-1201793) for more information.