Audit repository optimization - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 13.0.50

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document number
LIT-1201645
Version
13.0.50
Revision date
2024-02-26
Product status
Active

Optimize the required storage size of the ADS/ADX Audit repository by specifying the Audit level (1 through 4) for the audit messages that need to be reported and archived.

In addition, optimize the network communication performance for transferring audit messages from the engines to the ADS/ADX Event repository by optimizing the Audit repository size in the device object of each engine.

Audit Level 1 provides the minimum information. Audit Level 4 provides the most information. Audit Level 2 is the default setting. Refer to the Audit Trail topic in the Metasys SMP Help (LIT-1201793) for more information.