Audit repository database overview - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 13.0.50

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document type
Commissioning Guide
Document number
LIT-1201645
Version
13.0.50
Revision date
2024-02-26
Product status
Active

The Audit Repository resides on the ADS/ADX within the SQL Server software database.

The installation program places the Audit repository on the same computer where the ADS/ADX software resides. The default directory location is C:\ProgramData\Johnson Controls\MetasysIII\SQLData (pre-Release 8.0) or C:\Program Files\Microsoft SQL Server\MSSQL<version>.MSSQLSERVER\MSSQL\DATA (Release 8.0 or later). For a split ADX, the directory location is on the database server computer on the same drive where the SQL Server software is installed. If you want to change where the databases are loaded (for example, E:\MyDatabases), you need to do so before you install the ADS/ADX software. For details, refer to the Metasys Server Installation and Upgrade Instructions (LIT-12012162) or the Metasys Server Lite Installation and Upgrade Instructions (LIT-12012258).