Printing information displayed on the user interface - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 13.0.50

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document type
Commissioning Guide
Document number
LIT-1201645
Version
13.0.50
Revision date
2024-02-26
Product status
Active

Any printer supported by the computer's operating system can be used to print the content of any panel displayed on the SMP user interface. The supported printers include IP network printers and printers connected using a USB or parallel port. Printing through Novell NetWare services is not supported.