The user interface organizes the ADS device object attributes in the tabs in the right pane. For a description of each tab, see Table 1. In the focus tab, the object type and model name of an ADX are both shown as ADS for the ADS device object.
|
Tab |
Purpose |
Online/SCT |
|---|---|---|
|
Focus/Configuration |
Description of device including information related to site. The tab also includes general information about the ADS repository, particularly if historical data needs to be forwarded to other ADS repositories. |
Both Note: The
Focus tab appears online and the Configuration tab appears in the SCT.
|
|
Summary |
Name, value, status, and description for trend study or user graphic items in the ADS |
Online |
|
Diagnostic |
HTTPS messaging information for diagnostic purposes |
Online |
|
|
Email configuration and destination information |
Both |
|
SNMP |
Simple Network Management Protocol (SNMP) configuration and destination information |
Both |
|
Syslog |
The syslog option provides positive indication of each field possible in the Metasys event and audit entries, replacing any blank field with the single character dash (-). |
Both |
|
Printer |
Alarm printer configuration and destination information |
Both |
| Network | Network configuration information | Both |
| Alarm | Alarm configuration information | Both |
| Trend | Trend information | Both |