ADS device object - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 13.0.50

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document type
Commissioning Guide
Document number
LIT-1201645
Version
13.0.50
Revision date
2024-02-26
Product status
Active

The user interface organizes the ADS device object attributes in the tabs in the right pane. For a description of each tab, see Table 1. In the focus tab, the object type and model name of an ADX are both shown as ADS for the ADS device object.

Figure 1. ADS Device Object in SMP and Metasys UI



Note: In the following table, online refers to the tabs you see when you look at the ADS/ADX user interface. SCT refers to the tabs you see when you look at an archive database in the SCT. The Summary tab is available in Metasys UI as a separate Summary widget.
Table 1. User interface tabs of the ADS device object

Tab

Purpose

Online/SCT

Focus/Configuration

Description of device including information related to site. The tab also includes general information about the ADS repository, particularly if historical data needs to be forwarded to other ADS repositories.

Both

Note: The Focus tab appears online and the Configuration tab appears in the SCT.

Summary

Name, value, status, and description for trend study or user graphic items in the ADS

Online

Diagnostic

HTTPS messaging information for diagnostic purposes

Online

Email

Email configuration and destination information

Both

SNMP

Simple Network Management Protocol (SNMP) configuration and destination information

Both

Syslog

The syslog option provides positive indication of each field possible in the Metasys event and audit entries, replacing any blank field with the single character dash (-).

Both

Printer

Alarm printer configuration and destination information

Both

Network Network configuration information Both
Alarm Alarm configuration information Both
Trend Trend information Both