Time synchronization methods - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 13.0.50

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document type
Commissioning Guide
Document number
LIT-1201645
Version
13.0.50
Revision date
2024-02-26
Product status
Active

Three methods for network time synchronization are available in the Metasys system, including Windows Simple Network Time Protocol (SNTP) time synchronization, Multicast, and BACnet® time synchronization.

You can use the Microsoft Windows and Multicast methods when an SNTP master time server is available. If the Site Director has no access to SNTP time servers, you can use the BACnet synchronization method.

To enable a time synchronization method, modify the Time Sync Method attribute for the Site. See the Steps for successful time management and Setting the time synchronization method sections.