Example network - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 13.0.50

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document type
Commissioning Guide
Document number
LIT-1201645
Version
13.0.50
Revision date
2024-02-26
Product status
Active

Figure 1 shows an example system with a common time zone, date, and time management setup. This example is representative of the Multicast and Windows time synchronization methods.

The Site Director is configured to receive the date and time from an intranet time server. The date and time originates at an Internet time server (such as the Naval atomic clock). Using Simple Network Time Protocol (SNTP), the intranet time server requests the time from the Internet time server. The Site Director requests the time from the intranet time server. Then, using the Metasys system automatic time synchronization, and the manually configured time zone, the Site Director automatically provides the time zone, date, and time to the other engines/server on the Metasys network.

Figure 1. Time Management Sample System