Managing preferences - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 13.0.50

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document type
Commissioning Guide
Document number
LIT-1201645
Version
13.0.50
Revision date
2024-02-26
Product status
Active

Beginning with Metasys Server at Release 8.0, user preferences (and object lists) that are created on the ADS/ADX are saved in the archive database by SCT. They are part of the archive upload/download process, so you no longer need to save these xml files before an upgrade. However, system preferences on the ADS/ADX are not archived in SCT, so you still must manage these files manually during an upgrade.

For information on managing preferences for each preference type, see the following sections: