Copying preferences between devices - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 13.0.50

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document number
LIT-1201645
Version
13.0.50
Revision date
2024-02-26
Product status
Active

Procedure

  1. Access the source Metasys system device; that is, the one that contains the preferences you want to copy.
  2. Navigate to the Preferences directory for the device as shown in Table 1.
  3. Copy SystemPreferences.xml (system preference) or UserPreferences-userID.xml (user preference), where userID is the identification number that appears in the Security Administration tool.
  4. Paste the file onto the desktop of your computer.
  5. If you are accessing the Metasys system device remotely, log out.
  6. Access the destination Metasys system device (where you want to copy the preferences) as the MetasysSysAgent user and navigate to the Preferences directory for the device as shown in Table 1.
  7. Paste the SystemPreferences.xml file or UserPreferences-userID.xml file that you copied to your computer desktop with Step 4.