Configuring and maintaining preferences introduction - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 13.0.50

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document number
LIT-1201645
Version
13.0.50
Revision date
2024-02-26
Product status
Active

The Metasys system provides customized preferences for the user interface. The preferences allow authorized users to configure how the user interface behaves, including the sounds and colors, the startup view, and the ability to add links to external applications that can be accessed from within the user interface of the ADS/ADX/SCT device.

Important: Preferences do not persist after an upgrade unless you take manual steps to save the settings before you begin a system upgrade. See Preserving preferences in an upgrade.

Some steps in the following sections involve certain file operations, such as copying files and navigating to specific folders. The tool used for these operations is Windows File Explorer (ADS/ADX ), .