Renaming the computer - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 13.0.50

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document number
LIT-1201645
Version
13.0.50
Revision date
2024-02-26
Product status
Active
  1. To access the Metasys Rename Assistant, see Starting the Metasys Rename Assistant
  2. Click Windows Rename in the Metasys Rename Assistant.
  3. In the System Properties window, click Next.
  4. Click the Computer Name tab.
  5. Click Change.
  6. In the Metasys Rename Assistant, click Next. In the Computer Name/Domain Changes window, in the Computer name field, enter the new ADS name. This name appears in red text in the Metasys Rename Assistant.
    Note:
    • If this computer is a member of a domain, specify the name in the Domain field. If the computer name includes a DNS suffix, enter the suffix.
    • If you join the computer to a domain, the DNS suffix appears automatically. If you join the computer to a workgroup, the DNS suffix is optional.
  7. Click Next in the Metasys Rename Assistant. Click OK.
  8. Click Next in the Metasys Rename Assistant. Click OK in the Computer Name/Domain Changes window.
    Note: You must restart your computer to apply these changes.
  9. Click Next in the Metasys Rename Assistant. Close all windows other than the Metasys Rename Assistant.
  10. Click Next in the Metasys Rename Assistant. Click OK when you are prompted to restart the computer.