Downloading the Metasys archive database - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 13.0.50

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document number
LIT-1201645
Version
13.0.50
Revision date
2024-02-26
Product status
Active
  1. Click Launch SCT.
  2. In the Metasys Launcher, click the SCT tab, select the server, and then click Launch.
  3. Select the archive that you performed an upload to in Preparing the archive database.
  4. In the Metasys Rename Assistant, click Next.
  5. In the Metasys Rename Assistant, click Next, and then in the SCT, click the Metasys server in the navigation tree.
    Note: It is normal at this time for the site name to be the same as the original ADS name. Do not attempt to change the site name at this time.
  6. In the Metasys Rename Assistant, click Next, and then in the SCT, from the Tools menu, click Manage Archive.
  7. In the Manage Archive wizard, click Next.
  8. On the Action page, click Download to Device, select the Include Security checkbox, and then click Next.
  9. In the Metasys Rename Assistant, click Next, and then in the SCT, complete the following steps:
    1. On the Select Devices page, select the devices to download, and then click Next.
    2. On the Schedule page, if you need to schedule the download for a later time, select the appropriate download time, and then click Next.
    3. On the Device Change page, clear the Use this option to rename a device through the download process checkbox and the Use this option to change a device address during the download checkbox, and then click Next.
  10. In the Metasys Rename Assistant, click Next, and then in the SCT, complete the following steps:
    1. On the Site Login page, click Test Login.
    2. Click Next.
    3. Click Next.
    4. Click Finish.
    5. Close the SCT.