Appendix: Changing the ADS or ADX name and the computer name on an ADS and unified ADX - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 13.0.50

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document number
LIT-1201645
Version
13.0.50
Revision date
2024-02-26
Product status
Active

Follow the steps in this section to change the name of an ADS/ADX . The ADS/ADX name and the computer name must match for proper functionality.

Important: After you follow these procedures for a Site Director, the fully qualified item references have the new ADS/ADX name and do not match the fully qualified item references in historical data. For tools that access historical data, such as the Metasys Export Utility, you may need to use the old item references to retrieve data.
Important: Do not follow these instructions for an ADS/ADX Turnkey computer. To rename an ADS/ADX Turnkey computer, refer to Appendix: Changing the ADS/ADX Name and the Computer Name of the ADS/ADX Turnkey User's Guide (LIT-12011177) .