ADS/ADX and SCT temporary file cleanup - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 12.0

ADS/ADX Commissioning Guide

Brand
Metasys
Product name
ADS Server
ADX Server
Document type
Commissioning Guide
Document number
LIT-1201645
Version
12.0
Revision date
2022-09-22
Product status
Active
Language
English

Computers with ADS/ADX and SCT software generate temporary and transient files related to the operation of the ADS/ADX and SCT. These files can accumulate and reduce the available hard disk space. You can delete or move these files offline to help save on hard disk space.

The Metasys system folders with temporary and transient files are either located in C:\Users\All Users\Johnson Controls\MetasysIII or C:\ProgramData\Johnson Controls\MetasysIII.

The particular subfolders that contain temporary or transient content are:

  • \Diagnostics
  • \download
  • \FileTransfer
  • \SecurityFiles
  • \temp
  • \upload

When you delete or move the files under these folders, do not delete or move the folders themselves, just the subfolders and any files under the subfolders. Also, do not disturb any other MetasysIII folders that are not listed here.