|
Recommended computer platform 1 |
Intel i7 processor latest version with at least 6 cores or better 2 x 500 GB hard disk (RAID 1)
2 with 40 GB free space after installation of all prerequisite software and before installation of ADS-Lite software. Configure RAID 1 (mirroring) with disk write-caching turned on.
Note: Prerequisite software includes the supported operating system, database software, .NET Framework, and any other software or service packs required for your ADS configuration.
Graphics adapter (1 GB RAM, ATI® Technologies or NVIDIA® Corporation, 64-bit compatible [for 64-bit operating systems], Small Form Factor [SFF] if required) |
|
|
Required minimum memory 3 |
8 GB minimum, 16 GB recommended The VM host must have at least 8 GB of allocated RAM at all times. When you configure the VM, do not select the enable dynamic memory option. |
|
|
Supported operating systems and database software 4 |
Windows® 10 Pro and Windows 10 Enterprise Editions versions 2004, 21H1, and 21H2 (64-bit). For all future Windows 10 updates after version 21H2, we will evaluate and certify that Metasys software can support the updates before we provide guidance on support. Windows® 10 Enterprise LTSC (21H2) (64-bit)Database software:
|
|
|
Supported virtual environments |
Microsoft Hyper-V™ VMware® |
|
|
Supported user interfaces |
Site Management Portal (SMP) Metasys UI Note:
SMP requires a license at Release 12.0. The
license is available only to existing Metasys
customers.
|
|
| Additional software included with the ADS Lite software download |
Microsoft .NET Framework 4.7.2 Microsoft .Net Core 3.1.21 Launcher Software |
|
|
Optional hardware |
Any network or local printer supported by the qualified Windows operating system |
|
|
Optional software |
Graphic Generation Tool CCT Software SCT Software Metasys Database Manager Metasys Export Utility |
|
1 Our computer platform and memory
recommendations are not meant to imply that older or slower
machines are not usable. Refer to the
Network and IT Guidance Technical Bulletin (LIT-12011279)
1 for
more information regarding computer/server
recommendations.
2 For best performance, use Serial Attached SCSI (SAS) hard drives, not Small Computer System Interface (SCSI) hard drives.
3 It is recommended to use RAM that the
computer supports.
4 Refer to the
Network and IT Guidance Technical Bulletin (LIT-12011279)
for specific Microsoft Windows
operating system settings that may be required for your
Metasys system configuration.