Configuring Metasys Advanced Reporting System settings - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 12.0

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document number
LIT-1201645
Version
12.0
Revision date
2022-09-22
Product status
Active

The administrator of the reporting system ADX can manually refresh data and modify default settings on the ADX such as changing the timeout period and the default number of rows allowed in a report.

The settings in this section reset to their default values when you upgrade or uninstall/reinstall the ADX software. Reconfigure the settings as desired.