Site Director - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 12.0

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document number
LIT-1201645
Version
12.0
Revision date
2022-09-22
Product status
Active

The Site Director provides all users a uniform point of entry to the system and the ability to view all network components, including the information defined in the site object. The Site Director supports functions such as user login, user administration, and time synchronization.

On a Metasys site, only one ADS/ADX server can be configured as the Site Director. All User Views created for a site need to reside on the ADS/ADX configured as the Site Director. Typically, the user graphics created for a site also reside on the Site Director ADS/ADX .

Note: From Release 10.0, it is not possible to configure a connection to a cloud-based platform with the attributes in the remote services connection table of the site object.