Audit repository optimization - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 12.0

ADS/ADX Commissioning Guide

Brand
Metasys
Product name
ADS Server
ADX Server
Document type
Commissioning Guide
Document number
LIT-1201645
Version
12.0
Revision date
2022-09-22
Product status
Active
Language
English

Optimize the required storage size of the ADS/ADX Audit repository by specifying the Audit level (1 through 4) for the audit messages that need to be reported and archived.

In addition, optimize the network communication performance for transferring audit messages from NAE/NCE or NIE devices to the ADS/ADX Event repository by optimizing the Audit repository size in the device object of each engine.

Audit Level 1 provides the minimum information. Audit Level 4 provides the most information. Audit Level 2 is the default setting. Refer to the Audit Trail topic in the Metasys SMP Help (LIT-1201793) for more information.