Printing information displayed on the user interface - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 12.0

ADS/ADX Commissioning Guide

Brand
Metasys
Product name
ADS Server
ADX Server
Document type
Commissioning Guide
Document number
LIT-1201645
Version
12.0
Revision date
2022-09-22
Product status
Active
Language
English

Any printer supported by the computer's operating system can be used to print the content of any panel displayed on the SMP user interface. The supported printers include IP network printers and printers connected using a USB or parallel port. Printing through Novell NetWare services is not supported.