Windows time synchronization - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 12.0

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document type
Commissioning Guide
Document number
LIT-1201645
Version
12.0
Revision date
2022-09-22
Product status
Active

The Windows time synchronization is Microsoft Corporation’s implementation of the standard Windows SNTP w32time. This method is also referred to as unicast synchronization. With this form of time synchronization, all routers can route User Datagram Protocol (UDP) traffic. Windows time synchronization may have a larger time interval in which devices are out of sync with the SNTP master time server due to skewing and convergence.

If you use Windows time synchronization, you must define a device time server in the Site Director using the Device Time Servers attribute.

Note: If you implement an intentional time change for your site, in less than 5 minutes, all other devices on the site update with the new time with Windows time synchronization.