BACnet time synchronization - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 12.0

ADS/ADX Commissioning Guide

Brand
Metasys
Product name
ADS Server
ADX Server
Document type
Commissioning Guide
Document number
LIT-1201645
Version
12.0
Revision date
2022-09-22
Product status
Active
Language
English

BACnet time synchronization uses BACnet protocol to synchronize with BACnet devices such as the network engine. Use this method when the Site Director has access to a BACnet time server. This method is not available on the Metasys server.