Setting the date and time in the Site Director ADS/ADX - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 12.0

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document number
LIT-1201645
Version
12.0
Revision date
2022-09-22
Product status
Active

About this task

Before manually setting the date and time in the Site Director ADS/ADX , follow the steps in the Setting the time zone in the Site Director ADS/ADX section.

Procedure

  1. Click the time in the lower-right corner of the screen. Click Change date and time settings.
  2. Set the time and date.
  3. Click OK.

    The Site Director time zone, date, and time are now set and propagate to all other engines/servers on the site.