ADS/ADX as Site Director - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 12.0

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document number
LIT-1201645
Version
12.0
Revision date
2022-09-22
Product status
Active

Set the time zone first, then either set the date and time or select a time server for the Site Director.

See the Verifying the Site Director defined for an engine/server and Setting the time synchronization method sections before following the steps in this section.

Notes:
  • If you select a site time server for your Site Director, and you also set the time manually in the ADS/ADX , the manual time is overridden at the end of the time specified in the Time Sync Period attribute (default is 1 hour).