Purchasing and designating operating system CALs - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 12.0

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document type
Commissioning Guide
Document number
LIT-1201645
Version
12.0
Revision date
2022-09-22
Product status
Active

You need to purchase one additional device CAL for every network engine added to your Metasys system. You may also need to purchase additional user CALs as you expand the number of authorized Metasys system users. If you currently have an ADS and you expand your system to require more than 10 connections, you must migrate to an ADX and purchase the appropriate number of CALs.

For CAL purchasing information, log in to the Johnson Controls employee portal website, go to the Tools & Applications page, then click the Computer Price List link in the Procurement/Purchasing section. This page contains the necessary information on how to access the Insight/Johnson Controls website (http://www.insight.com/jci) that contains information about purchasing CALs.

If Metasys system software is purchased separately, the customer is responsible for purchasing the correct number of CALs and for properly designating each CAL. A device CAL cannot be transferred to a user CAL, or vice versa. If a Metasys Ready computer is purchased, the proper number of operating system CALs come with the purchase, so no additional operating system CALs are required. Ultimately, the customer must determine how to split the total number of CALs between device or user.

For additional information on CALs, licensing, and downgrading operating system CALs, refer to http://www.microsoft.com/licensing/about-licensing/client-access-license.