Restoring default system preferences - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 12.0

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document number
LIT-1201645
Version
12.0
Revision date
2022-09-22
Product status
Active

Procedure

  1. Access the Metasys system device on which you want to restore the default system preferences.
  2. Navigate to the Preferences directory for the device as shown in Table 1.
  3. Delete the SystemPreferences.xml file.