Applying the ADS/ADX settings - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 12.0

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document number
LIT-1201645
Version
12.0
Revision date
2022-09-22
Product status
Active
  1. Click Launch ADS/ADX .
  2. Click Next and close all user views.
  3. In the Metasys Rename Assistant, click Next, and then in the ADS/ADX Site Management Portal (SMP), from the View menu, click Extended Labels.
  4. In the Metasys Rename Assistant, click Next, and then in the SMP, double-click the Metasys site in the navigation tree.
  5. In the Metasys Rename Assistant, click Next, and then in the SMP, click Edit in the Display pane.
  6. In the Metasys Rename Assistant, click Next, and then in the Site View tab in SMP, in the Name attribute, enter the new server name.
    Note: The name is case sensitive.
  7. In the Metasys Rename Assistant, click Next.
  8. In the SMP, in the Time Zone attribute, set the time zone to the zone that is displayed in the Metasys Rename Assistant.
  9. In the Metasys Rename Assistant, click Next, and then in the SMP, click Save.
  10. In the Metasys Rename Assistant, click Next, and then in the SMP, from the Action menu, click Refresh All Tabs.
  11. In the Metasys Rename Assistant, click Next, and exit the SMP.
  12. In the Restart Computer Now window, click Next, and then click OK.