Description - Johnson Controls - LIT-12013929 - ZPS Zone Presence Sensor

ZPS100 Zone Presence Sensor Data Sheet

Product name
ZPS Zone Presence Sensor
Document type
Datasheet
Document number
LIT-12013929
Revision date
2021-10-22
Figure 1. ZPS100 zone presence sensor

The ZPS100 Zone Presence Sensor, part of the complete fume hood solution, provides economical fume hood usage without compromising safety.

Using its microwave motion sensor, the attached controller is instantly instructed to switch to OCCUPIED mode once an operator is in front of the fume hood. Unattended fume hoods revert to an UNOCCUPIED status after a user-specified number of minutes expire, thereby saving energy.

Highly sensitive and accurate, the ZPS100 is capable of detecting motion down to 1/4” per second. In addition, the ZPS100 can be tailored for any size fume hood. Sensitivity and time delay are also configurable on the ZPS and associated hood controller.