Status indication LEDs - Johnson Controls - WT-ROUTER - Digital Thermostat - Pneumatic to DDC Thermostat - Pneumatic Thermostat - WT-ROUTER Router

WT-ROUTER Router Installation Guide

Product
Network and Communications > Gateways and Routers > WT-ROUTER Router
Document type
Installation Guide
Document revision
B
Revision date
2020-04-07
Part number
24-10732-13

The WT-ROUTER communicates status using the following LEDs:

  • STS LED—Blinking indicates that the router is connected to the wireless network with only one active path. This LED remains on if two or more wireless paths exist.
  • ACT LED—On steady indicates that there is RF traffic at the device.
  • PWR LED—On steady indicates that power is applied to the device.