Mounting - Johnson Controls - WT-ROUTER - Digital Thermostat - Pneumatic Thermostat - Pneumatic to DDC Thermostat - WT-ROUTER Router

WT-ROUTER Router Installation Guide

Product
Network and Communications > Gateways and Routers > WT-ROUTER Router
Document type
Installation Guide
Document revision
B
Revision date
2020-04-07
Part number
24-10732-13

The WT-ROUTER Router can be surface mounted using two field-furnished screws. Mount the unit to the surface at the two mounting hole locations on the device (Figure 1).

The router can also be secured to a bracket above a drop ceiling using field-furnished tie wraps.