Character Sets Supported - Johnson Controls - LIT-12011936 - Gateway/Router

WT-BAC-IP Gateway Protocol Implementation Conformance Statement Technical Bulletin

Brand
Johnson Controls
Document type
Technical Bulletin
Document number
LIT-12011936
Revision date
2018-06-29
Language
English

Indicating support for multiple character sets does not imply that they can all be supported simultaneously.

ANSI X3.4 IBM®/ Microsoft® Double-Byte Character Set (DBCS) ISO 8859-1
ISO 10646 Universal Character Set-2 (UCS-2) ISO 10646 (UCS-4) Japanese Industrial Standard (JIS) C 6226

If this product is a communication gateway, describe the types of non BACnet equipment/network(s) that the gateway supports:

Modbus®

Table 9 lists all the BACnet standard application services. The checked services are supported by the WT-BAC-IP Gateway.

Table 1. BACnet Standard Application Services Support
Application Service Initiates Requests Executes Requests
AcknowledgeAlarm
AddListElement
AtomicReadFile
AtomicWriteFile
ConfirmedCOVNotification
ConfirmedEventNotification
ConfirmedPrivateTransfer
ConfirmedTextMessage
CreateObject
DeleteObject
DeviceCommunicationControl
Disconnect-Connection-To-Network
Establish-Connection-To-Network
GetAlarmSummary
GetEnrollmentSummary
GetEventInformation
I-Am
I-Am-Router-To-Network
I-Could-Be-Router-To-Network
I-Have
Initialize-Routing-Table
Initialize-Routing-Table-Ack
LifeSafetyOperation
ReadProperty
ReadPropertyConditional
ReadPropertyMultiple
ReadRange
ReinitializeDevice
RemoveListElement
SubscribeCOV
SubscribeCOVProperty
TimeSynchronization
UnconfirmedCOVNotification
UnconfirmedEventNotification
UnconfirmedPrivateTransfer
UnconfirmedTextMessage
UTCTimeSynchronization
VT-Close
VT-Data
VT-Open
Who-Has
Who-Is
Who-Is-Router-To-Network
WriteProperty
WritePropertyMultiple