Document Introduction - Johnson Controls - LIT-12011936 - Gateway/Router

WT-BAC-IP Gateway Protocol Implementation Conformance Statement Technical Bulletin

Brand
Johnson Controls
Document type
Technical Bulletin
Document number
LIT-12011936
Revision date
2018-06-29
Language
English

This document contains the Protocol Implementation Conformance Statement (PICS) and BACnet® Interoperability Building Blocks (BIBBs) for theWT-BAC-IP Gateway as required by the American National Standards Institute/American Society of Heating, Refrigerating, and Air-Conditioning Engineers (ANSI/ASHRAE) Standard 135-2001, BACnet protocol.

The PICS is a written document created by the manufacturer of a device to identify the particular options specified in the BACnet standard and implemented in the device.

BACnet Interoperability Building Blocks are collections of one or more BACnet services. This document includes a listing of the BIBBs currently supported by the WT-BAC-IP Gateway.