Mesh mode - Johnson Controls - WRZ-THJ - WRZ-THN - WRZ-TTJ - WRZ-TTK - WRZ-TTP - WRZ-TTR - WRZ-TTS - Wireless Device - WRZ one-to-one Wireless Room Sensing System

WRZ Series Wireless Room Sensors Installation Guide

Brand
Johnson Controls
Product name
WRZ one-to-one Wireless Room Sensing System
Document type
Installation Guide
Part number
24-10332-2
Document revision
V
Revision date
2020-07-09
Language
English

You can add up to nine WRZ Series Sensors to each Controller in the mesh mode.

The Zone DIP switches on the WRZ Sensor relate to the Zone Netsensor (SA bus device) address configured for the sensor in the Controller Configuration Tool (CCT). For example, if you set the Zone DIP switches to a value of 3 with DIP switch 1 and DIP switch 2 set to ON, you must use Zone Netsensor address 202 in the CCT. You can add up to nine WRZ Sensors to each field controller. You can use any nine of the sixteen available Zone Netsensor address settings at a time.

The mesh mode of operation is intended for use with the ZFR or ZFR Pro Series Coordinator and ZFR or ZFR Pro Series Router. Table 1 describes the Zone DIP switch settings for the wireless applications in mesh mode.

Table 1. Zone Switch and SA bus settings when using multiple WRZ Sensors
Zone DIP Switch ON1 Zone Netsensor (SA bus device) address setting
None (All OFF) 199
1 200
2 201
1 and 2 202
4 203
1 and 4 204
2 and 4 205
1, 2, and 4 206
8 207
1 and 8 208
2 and 8 209
1, 2, and 8 210
4 and 8 211
1, 4, and 8 212
2, 4, and 8 213
1, 2, 4, and 8 214
1 Use the one-to-one application DIP switch overlay in the one-to-one mode of operation, or the mesh application DIP switch overlay in the mesh mode of operation. The switch numbers described in this table refer to the numbers on the overlays.