Temperature sensor considerations - Johnson Controls - WRZ-THJ - WRZ-THN - WRZ-TTJ - WRZ-TTK - WRZ-TTP - WRZ-TTR - WRZ-TTS - Wireless Device - WRZ one-to-one Wireless Room Sensing System

WRZ Series Wireless Room Sensors Installation Guide

Brand
Johnson Controls
Product name
WRZ one-to-one Wireless Room Sensing System
Document type
Installation Guide
Part number
24-10332-2
Document revision
V
Revision date
2020-07-09
Language
English

To locate a WRZ Series Sensor, follow the same best practices used to locate a hard-wired temperature control, sensor, or thermostat:

  • Mount the sensor on an interior wall where it is easily accessible, at least 1.4 m (55 in.) above the floor, in an area where the temperature is representative of the entire controlled space.
  • Avoid enclosed or recessed locations and locations behind curtains, doors, or other obstructions to the controlled space.
  • Avoid locations near entry foyers, doors, windows, supply air ducts, and pipes.
  • Avoid locations exposed to drafts, direct sunlight, and other sources of heat or cold.
  • Avoid locations exposed to excessive vibration.