Removing a mounting base installed with double-sided adhesive foam tape - Johnson Controls - WRZ-THJ - WRZ-THN - WRZ-TTJ - WRZ-TTK - WRZ-TTP - WRZ-TTR - WRZ-TTS - Wireless Device - WRZ one-to-one Wireless Room Sensing System

WRZ Series Wireless Room Sensors Installation Guide

Brand
Johnson Controls
Product name
WRZ one-to-one Wireless Room Sensing System
Document type
Installation Guide
Part number
24-10332-2
Document revision
V
Revision date
2020-07-09
Language
English

About this task

To remove or relocate a sensor mounted with double-sided adhesive foam tape, complete the following steps:

Procedure

  1. Remove the sensor housing from its mounting base. See Figure 1.
  2. Carefully twist the base off of the surface to remove the mounting base from the mounting surface.
  3. Remove the adhesive foam tape from the mounting base and clean the mounting base to remove any leftover adhesive.
    Note: New double-sided adhesive foam tape is required to remount the base on the surface. Use Can-Do National Tape (Code No. 99116) adhesive foam tape or its equivalent.