Repair information - Johnson Controls - WRZ-STR0000-x - WRZ-STRNIST-2 - Wireless Device - WRZ One-to-One Wireless Room Sensing System

WRZ-STR0000-x Series Wireless Refrigerator or Freezer Temperature Transmitter and Probe Assemblies Installation Guide

Product name
WRZ One-to-One Wireless Room Sensing System
Document type
Installation Guide
Document revision
H
Revision date
2020-07-09

If the WRZ-STR0000-x Series Wireless Refrigerator or Freezer Temperature Transmitter and Probe Assembly fails to operate in its specifications, replace the unit. For a replacement assembly, contact the nearest Johnson Controls representative.

Note: The temperature sensor probe can be ordered separately from the transmitter assembly. See Table 1 for ordering information.