Temperature sensor probe considerations - Johnson Controls - WRZ-STR0000-x - WRZ-STRNIST-2 - Wireless Device - WRZ One-to-One Wireless Room Sensing System

WRZ-STR0000-x Series Wireless Refrigerator or Freezer Temperature Transmitter and Probe Assemblies Installation Guide

Brand
Johnson Controls
Product name
WRZ One-to-One Wireless Room Sensing System
Document type
Installation Guide
Part number
24-10332-10
Document revision
H
Revision date
2020-07-09
Language
English

To locate the temperature sensor probe, follow these guidelines:

  • Mount the probe inside the refrigerator or freezer unit away from the front, so as not to interfere with the stored contents and to eliminate any false temperature spikes when the door opens.
  • Run the 9 ft (2.7 m) wire lead through the door gap or an existing hole designed for remote temperature sensor probe installation.
Note: Do not use an existing hole designed for electrical voltage because this affects the temperature reading. Do not drill a hole through the wall of the refrigerator or freezer unit for the wire lead unless approved by the refrigerator or freezer manufacturer, and also approved by the customer.