Special tools needed - Johnson Controls - WRZ-STR0000-x - WRZ-STRNIST-2 - Wireless Device - WRZ One-to-One Wireless Room Sensing System

WRZ-STR0000-x Series Wireless Refrigerator or Freezer Temperature Transmitter and Probe Assemblies Installation Guide

Brand
Johnson Controls
Product name
WRZ One-to-One Wireless Room Sensing System
Document type
Installation Guide
Part number
24-10332-10
Document revision
H
Revision date
2020-07-09
Language
English
  • 1/16 in. (1.6 mm) Allen-head adjustment tool (Johnson Controls┬« T-4000-119; order separately) for the tamper-resistant set screw that secures the transmitter to the mounting base
  • Coin to unlock the transmitter housing from the mounting base locking tab