Batteries - Johnson Controls - WRZ-STR0000-x - WRZ-STRNIST-2 - Wireless Device - WRZ One-to-One Wireless Room Sensing System

WRZ-STR0000-x Series Wireless Refrigerator or Freezer Temperature Transmitter and Probe Assemblies Installation Guide

Brand
Johnson Controls
Product name
WRZ One-to-One Wireless Room Sensing System
Document type
Installation Guide
Part number
24-10332-10
Document revision
H
Revision date
2020-07-09
Language
English

The two AA alkaline batteries supplied with the WRZ Series Sensor have a life of 5-10 years or more, depending on the model and application. The transmitter reports a low battery condition to the receiver or controller, that relays the low battery condition to the system. The low battery condition is also shown on the LCD on the face of the transmitter.

Replace the transmitter batteries with two high-quality AA alkaline batteries as necessary. Ensure to install the batteries in the correct polarity. See Preparing the WRZ-STR0000-x Series Transmitter for operation.

Note: When you replace batteries, both batteries should be replaced at the same time. Batteries removed from this device must be recycled or disposed of in accordance with local, regional, and national regulations. Only certified technicians or qualified building maintenance personnel should service Johnson Controls products. Li-ion batteries can be substituted to extend sensor life, depending on the model and application. Do not mix lithium and alkaline batteries in this device.